Other Parts Discussed in Thread: INA333, ADS1146
hi
I am using the ADC to measure bipolar signal from hall sensor. The hall sensor internal circuit is resistive bridge structure.
The output of hall sensor:
Sense+ = 1.5V + 20mVpp
Sense- = 1.5V + 20mVpp
Previously, I used INA333 (the gain is set to 40) to offset, amplify, and convert to single-ended signal. The signal is then connected to single-ended ADC. However that ADC doesn’t have 50/60Hz noise rejection capability.
I checked ADC with 50/60Hz noise rejection capability from TI website and found ADS1146 has the fastest sampling rate. Is there any single-ended TI ADC with 50/60Hz noise rejection?
What is the best external conditioning circuit for the hall sensor output to interface it to ADS1146. If I use INA333 to convert the signal to single-ended and connect to ADS1146, what should be the gain of the INA333 so not to exceed common-mode signal range of the ADS1146?
ADS1146 will be powered by 3.4V analog supply. I will use external reference voltage for the analog reference
Thank you!