I am writing to the DAC5571 and then performing a read back to verify the value was written correctly. There is about 1 ms between the write and read operation. However, I get a NAK whenever I transmit the device address with the READ bit. Why am I getting a NAK? I am using the low speed I2C mode.