Other Parts Discussed in Thread: ADS1244, LM1117, ADS1254, OPA350, OPA335, CC2530
I am having an intermittent problem with the ADS1244. Most of the time, it works exactly as planned. However in some cases it draws a significant amount of current (sometimes up to 1 amp). I was breaking down my circuit and one thing I have noticed that may be different is the order of the supply voltages. Would it make a difference to receive the 5V analog Ref before the 3.3V digital Ref? What could also be happening to make the ADS1244 to heat up?
Thanks.