I need to convert a wide-bandwidth signal, using a rapidly varying sample clock. The ADS5463 accepts a sample clock from 20MHz to 500MHz using a pipelined converter, with 3.5 cycles of latency, producing parallel DDR LVDS output. My input sample clock will vary rapidly in frequency from about 50MHz to about 450MHz several times over a 10 microsecond period. I'm assuming that the DDR output clock (DRY) will match the sample clock (at half the frequency), even though the sample being output from the converter is 3.5 cycles delayed. Can this device manage such a rapidly-changing sample clock?