Hi,
I am looking for high speed ADC with sampling rate over 10 MHz to be interfaced with OMAP-L138. Main goal is to build data acquisition system to store large amount of data in SD card. I realized OMAP-L138 is using SPI mode to communicate with SD card. I tried to make one project which uses UPP, I2C and SPI peripherals together, but that didn't work may be because some parameters were overlapping and can't work together. Although I couldn't figure out what was wrong in there.
Now I am seeking advise to use any ADC with any interface which helps implementing SD card feature in OMAP-L138 EVM.
I will appreciate your help.
Thanks.
Tariq