Other Parts Discussed in Thread: CDCE62005, DAC3482, ADS4249
Hi,
I am using a DAC3482EVM with the version 3.8 EVM GUI. I have setup a configuration file for the DAC3482 & CDCE62005 from the EVM GUI and have loaded it into the EVM. The GUI is running and I can make adjustments to the CDCE62005 and see changes in the EVM HW as desired. The control screens of the DAC3482 appear to be in a predisposed state. This DAC setup is not what I want. When I attempt to make adjustments to any of the DAC control registers from the GUI fields the App just switches them back. And the App has not specifically loaded the registers I originally saved.
Originally I defined settings within the DAC GUI with the DAC physically powered off and saved those settings in a file (see below). When I load those settings with the DAC EVM powered on the GUI controls are stuck in this undesired state. What am I doing wrong?
Thanks in advance for advise on this issue.
Pete
x00 xF10A x01 x0000 x02 x8002 x03 xA000 x04 xFFFF x05 x0A60 x06 x2C00 x07 xFFFF x08 x0000 x09 x8000 x0A x0000 x0B x0000 x0C x05A6 x0D x05A6 x0E x05A6 x0F x05A6 x10 x3000 x11 x0000 x12 x0000 x13 x0000 x14 x0000 x15 x0000 x16 x3333 x17 x3333 x18 x205F x19 x10F4 x1A x4820 x1B x0800 x1C x0000 x1D x0000 x1E x1118 x1F x8886 x20 x4100 x22 x1B1B x23 x001F x24 x1000 x25 x7A7A x26 xB6B6 x27 xEAEA x28 x4545 x29 x1A1A x2A x1616 x2B xAAAA x2C xC6C6 x2D x0000 x2E x0000 x2F x0000 x30 x61A8 x7F x0004 CDCE62005 Registers Freq:19.200000MHz Address Data 00 80400020 01 801C0301 02 C1800302 03 C1840303 04 81400304 05 281C1A55 06 04BF09E6 07 151877F7 08 20001C08