Other Parts Discussed in Thread: ADS1158, OPA227
Just to confirm, in my application, I am using a 2.048V reference and bipolar input mode. Can I assume that my 16-bit input range is +/-1.06*2.048V=+/-2.17088V at the input? Further, does this represent +/-32768 or +/-65536 internally?
If I do not need to add gain between the input mux and the A/D (via the MUX OUT and ADC IN breakout pins) of the ADS1158, do I need to unity-gain buffer this path? Is there any advantage to doing so?
Thanks in advance,
Scott