Other Parts Discussed in Thread: ADS1292RECG-FE
Hello, I have 2 questions regarding the ADS1292RECG-FE PDK:
1. After installing the PDK's drivers and the pc application, I opened the firmware's source code (which is included inside the installation folder) in CCS v5.0.
The code "as is" doesn't built.
Is there another, updated code?. Is there a chance the the CCS version doesn't fit?
2. I have an MSP-FETU430IF emulator which according to it's wiki page fits my PDK and the MSP proccessor in it.
The problem is that the emulator has 14 pins JTAG connector.
Is it possible to connect the emulator to the PDK? If so, can you elaborate on which pin goes where?
Thank you very much,
Udi