This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

please help me to design with tlc5602

Other Parts Discussed in Thread: TLC5602

in my fpga, i output a 13MHZ clock to tlc5602 and tlc5602 connect a TV.  synchronously ,fpga output video signal from external  to tlc5602.

but i can not see  image on TV screen.

i guess the clock frequency is not right.but what is right frequency should be ?

  • A 13MHz clock is within the limits of the device (20MHz max) so I don't think this is the problem.  Verify that the clock levels are within datasheet specifications.  If there are further questions please submit a new post and provide a schematic to assist in troubleshooting.

    Regards,