This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS62P49 footprin

Other Parts Discussed in Thread: ADS62P49

Hi all,

I need to design a PCB board involving ADS62P49. Unfortunately, I couldn't find any PCB footprint for this device.

Since I am quite new in PCB design, I am not really confident in creating new PCB footprint.

If anyone have a footprint for ADS62P49, could you please share with me ? I am using Altium Designer 6

Your support would be much appreciated

Dennis

  • Dennis,

    I can only give you the PCB footprint in Allegro format since this is the tool used to design the ADS62P49 EVM. 

    Attached is the footprint and package information. 

    Regards, Paul

    ADS62P49.zip
  • Hi Paul,

    Thanks a lot for your response !

    Could you do me a favor ? is it possible to convert from .DRA to Power PCB file (.ASC) or Altium files using Allegro ?

    Thanks a lot !

    Dennis

  • Dennis,

    Unfortunately the Allegro version that we're using does not allow us to export or save to a .asc file.  I was able to create a .dxf file if that helps.  See attached.

    Regards, Paul

    ADS62P49.zip
  • Thanks Paul !

    By the way, I am having few question regarding the Front End design for the input 

    Here I refer to page 34 in ADS62PXXEVM user guide Literature Number: SLAU237A

     - normally for transformer-coupled front end, I only see center tap at secondary winding. Why do we have center tap at primary winding as well in this case ?

    - Why do we have capacitor (C15- 0.1uF) connected to center tap and shunt to ground ?

    - Since we dont know frequency properties of glitches, how do we design this RCR filter ?(R25 C65 R26) filter ?

    - if INP and INM swing symmetrically between VCM +- 0.5, how does it result in 2Vpp differential input swing (I think it is only 1Vpp) ? And I don't understand how R5 R6 and C12 work to bias INP and INM ?

     

    Thank you ! Dennis

  • Hi,

    For the center tap on primary as well as secondary windings, the EVM has the pad and connection just for flexibility to choose other transformers or baluns later that may be more suited for a particular application.  Most of the transformers we use will have a center tap only on the secondary, and the pad for the possible center tap on the primary has no connection on the transformer so there is no harm in the extra pad.  But there are a few transformers i have seen that have a center tap on both primary and secondary.  Our transformer footprint is just designed for flexibility.

    I think the center tap has the bypass cap to help filter out common mode noise.

    The optimal values of the RCR filter to filter out sampling noise is dependent on the sampling rate and input frequencies of interest.  The RCR filter is somewhat a low pass filter, so the values are to be chosen that the bandwidth of the RCR is flat for the desired input frequencies, and then to roll off above that.   We don't want the RCR circuit to attenuate the desired input frequencies, so we set the bandwidth accordingly (normally by leaving the R=50ohms and choosing the appropriate value of C) to pass the input and filter out above that, regardless of the sample rate.  The sampling glitches are caused by the rising and falling edges of the sample clock, so we do know a lot about what frequencies the sampling glitches wil have (harmonics of the clock) but still we have to let the RCR pass the desired input bandwidth and we don't need to pass anything above the input frequencies so we set the RCR according to input frequency.

    By definition, the *peak to peak* differential voltage is 2V if each side of the differential signal swings 1V each.  So if at any time you define the input voltage as the 'P' side minus the 'M' side, then this voltage can befrom +1.0V to -1.0V, so the peak to peak difference is 2V.  And if each side of the differential signal has a 1V swing around a common mode, then the swing is from 0.5V below common mode to 0.5V above common mode.

    In that schematic, R5, R6 and C12 is just another RCR filter, but only one of the RCR filters is to be soldered in at any one time.  If you look at the datasheet for the ADS62P49 in the applications section, there is a typical input circuit for high input frequency (figure97) and another circuit for low frequency (figure96) input.  One difference is that the RCR filter is before the series 15Ohm in one case and after the series 5 ohm in the other case.  We built the EVM to be able to support either circuit.  

    Regards,

    Richard P.

  • Hi Richard,

    Thank you very much for your clarification !

    However, regarding the RCR filter, I'm a bit confused:

    Let's say my inputs is below 200Mhz, so we should pay attention to figure 96 in the datasheet. According to your post, we have two RCR filters: R5R6C12 and R25R26C65 ; and we ONLY can solder one of them (not both) at any time. Am I right to say that ?

    Thank you!

    Dennis

     

  • Dennis,

    for the ADS62P49 you actually need both RCR filters.

    The first one (R5R6C12) is the 50ohm termination of the input transmission line. This also has the AC termination to the common mode voltage (VCM) of the ADS62P49.

    The second RCR filter (R25R26C65) is designed to take care of the charge kickback of the ADC internal front end itself. If you compare several of our CMOS ADCs you'll notice that this RCR filter will vary from device to device and it also depending on input frequency itself.

    Please let us know if you have any further questions.

    Thomas Neu