Hello,
I am presenting a somewhat blind question, my apologies up front. Recently Kang Hsia helped me by arranging a rework of a DAC3482EVM digital bus connector to a connector that would support an HSMC interface to an Altera FPGA board. He suggested that I contact a colleague of his this week regarding this rework, but I do not have a specific individual's name. The factory DAC3482EVM has a Samtec QTH family connector with two mechanical mounting [retention] pins protruding from it (I assume these are designed to mate with the TI TSW family of boards). These pins will conflict with the connector on Altera FPGA development boards (Samtec QSH family, standard). Kang arranged a rework of a DAC3482EVM with a "standard" type QTH connector (QTH-090-01-L-D-A) without the -RT1 retention pin option.
Kang was working to have a 2nd board reworked for me this past week. He is on travel this week I understand. I wanted to ask if anyone is aware if he was able to get the rework process started; I believe the rework was done by TI or a TI partner.
Is there anyone I should specifically talk with about this?
Thanks,
Pete Harbour