Hi there,
I'm working with the ADS1299 chip and trying to interface it with an Arduino library that I'm building. I've been searching through the datasheet for what determines the tCLK master clock period, but can't seem to find it. I see that the range is from 444 ns to 666ns. Is that range linearly mapped to the DVDD supply (2.7 V < DVDD < 3.6 V) shown at the top of the column of Figure 1 (Timing Requirements) on pg. 8 of the datasheet?
If somebody could help me with this one, that would be great.
Thanks in advance.
Conor