This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

vedio decoder IC

Other Parts Discussed in Thread: TVP5146, TVP5150

Does anyboby know that what kind of IC that can be used in my application? The applicatioin is as:

  Input: composite TV signal(PAL, NTSC) which is interlaced mode

 Output: Progressive mode @ resolution 640X480 or 320*240 or even less

Holly

  • Hi Holly,

    I think most of the modern-time video decoders have an inherent input/output type selection facility.

    This can allow you to select either interlaced /progressive mode for input/output, the conversion will be internal.

    Your choices could be TVP5146, TVP5150 or ADV7188

    Regards,

    Sid