Hello,
I have an ADS4245 EVM. I want to use CMOS mode on this board which output from J1. In order to use CMOS mode, I just follow the datasheet 'User's Guide ADS42xx EVM' on page 9. Installed 'SN74AVC16T245' to U12 and U13; removed soldered resistors RN5 to RN12; and shunt JP26 and JP27. And then connect JP14 to 2's comp CMOS. All other connections are default.
After I connected to 125MHz clock and 1MHz signal. I don't see any output from J1. and the J1 pin 39 has a clock output which looks like a triangle form and peak to peak is about 25mV. Do I miss anything to run CMOS mode?
I tested 3-state buff's power supply. VCCA&VCCB are DC 3.3V and both ~OE are DC 0. I test output from main chip ADS4245 'DA11 DA10...'. The voltage level is very low which is less than 100mV.
I think I miss some setting on the board, but I can't find where I miss.
Thanks!
Zaidi