Hi there,
My TVP5150AM1 application does not colour lock on NTSC, but does on PAL.
Luminance is always correctly decoded.
Sometimes Pr is correctly decoded, but in that case there is no Pb.
Some background information:
The device is clocked from the crystal output of a 3.3V 8051-family device, running with a 14.31818MHz crystal.
I do have anti-alias filters as described in the application data.
I do allow for SCL stretching (software IIC interface) and delay-before-stop.
NTSC is included in the Auto-switch.
Reading back from the chip I find that register 0x88, bits 3::1 are all 1 (Colour, VS and HS all locked).
Register 0x8C reads back as 0x81 for NTSC and 0x83 on PAL.
I've tried running the device from its own crystal, but there is no difference in performance. I am at a loss as to where to go from here.
Any assistance appreciated.
Cheers,
Dave