Can I use a step-up transformer to drive the inputs of a non-buffered, wide bandwidth ADC? Something on the order of a 4:1 ratio? Also, how does the signal bandwidth and IF affect if such a set-up can provide good performance?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can I use a step-up transformer to drive the inputs of a non-buffered, wide bandwidth ADC? Something on the order of a 4:1 ratio? Also, how does the signal bandwidth and IF affect if such a set-up can provide good performance?
Dear Mr. Sanna-tizer,
If you are in the 1st 100MHz or so, it might be possible, if the target matching impedance is 25ohms, maybe 50. At higher frequencies or target impedances, the non-buffered ADC's impedance is falling too quickly. Simulations suggest with a buffered ADC and a target of 50ohms, still might be limited to first 100Mhz or so. But, it depends on how much gain droop across your band and how high a VSWR you can tolerate.
thanks for your interesting question,
Philip Pratt