@Matt, I am working with a pressure transducer that outputs 0-30mV and am having some trouble. I have a gain = 65x and when the pressure outputs 15mv x 65 gain = ~1V the INA333 appears to saturate. It will no longer bump up the voltage beyond this 1v (really is ~916mV). The input supply is 3.3V and the pressure sensor is the RTOP100A7 from Sensortechnics (http://www.sensortechnics.com/download/DS_Standard-RTO_E_11714_A.pdf). The INA333 is tied to an MCP3421 ADC. Any help on trouble shooting this would be appreaciated.