Is there somewhere I can get the source code for the MSP430 that is on the AFE4400 SPO2EVM? I would like to be able to capture the output directly into a terminal program so I can post-process the raw data. I have it reporting to a terminal but I don't see the data format described anywhere. I figured the source code would help, and I could also modify it to pre-process some items, if desired.
Essentially I would like to bypass the AFE44X0 GUI. Is this easy to do and I'm just missing how I am supposed to do it?