Other Parts Discussed in Thread: ADS62P42
Hi,
I presently have in hand a ADS62P42 EVM REV.B. What i would like to accomplish is to use your eval board but write myself into the registers without using the usb interface or parallel options available with the jumpers. I would like to do it with the Rasberry Pi using his GPIO pins and bit-banged the data to the registers managing the RESET, SCLK, SEN and SDATA inputs. I would like to know if it's possible to connect on the second pin where are located JP8, JP9, JP10 and JP11, disconnect those jumpers and supply the 5V_AUX_IN(P5)? From the schematics, it seems possible but i wanted to double check. Thanks a lot !