I have few question regarding ADC12D1800RFRB. I am considering using it for my application. Would be grateful if anyone can answer me
a) I want to capture pulsed analog signal ( voltage) that has pulse width of ~ 100 ns and has repetition rate of 1KHz. (1Khz..ie 1 ms gap between each pulse,1000 pulse per sec) . Can I capture such analog signal using ADC12D1800RFRB for continuously 10 sec and at the same time stream that data ( in REALTIME) samples ( of 10 sec) to save in Hard Drive ?
b) Is there any way to trigger the board and just capture data for that 100 ns in each cycle and save that data in HDD in real time ( or atleast all the pulses data ) for each cycle. ( Then how to tell the board to capture only 100ns after trigger in each cycle ? )
c) If it not possible then is it because of the software ( Wavevision 5) ? or itself the hardware is not capable for doing such thing ( so long continuos storage ) .
d) Is it possible to steam the data trough LVDS bus and save in another FPGA board with big memory ( say 2GB ) ?
e) Is it possible to write VB.net (or VC#) program using Wavevision DLL to do that function mentioned above.