This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ads5281- single data rate output or single ended outputs

Other Parts Discussed in Thread: ADS5281

Hey Richard,Kw Nam 

Got some hope which am actually looking for .........

I guess we can configure ADS5281 to single data rate 0r single ended outputs ..... see page no:18 in that go to LVDS OUTPUT TIMING then we can find it 

 it is shwon that sdr rate http://www.ti.com/lit/ds/symlink/ads5281.pdf

and should configure ad clk as single ended and L clk to be 12 times of that..

what do you say experts??? am i going anything wrong in that

regards

sahitya venkatayog

  • Hi, Sahitya

    This is regarding input clock interface which can be configured single ended CMOS or differential LVDS. The output of ADS5281 is still differential LVDS and this cannot be done with single ended.

    Thanks,

    KW