Other Parts Discussed in Thread: TVP5150AM1, TMS320DM368, TVP5150
hello i am interfacing tvp5150am1 with tms320dm368 processor via bt656 protocol
input of tvp5150 i have connected two composite video cameras
camera 1: CAMERA RESOLUTION: 640 x 512 / 640 x 480 / 512 x 512 or programmable Up to 60 Hz full frame rate.
camera 2: Approx. 440K pixels
Horizontal resolution
550 TV lines (WIDE end)
what will be the maximum frame per second (fps) i will get on BT656 end considering SCLK is 27Mhzs