Hi
Have you tried taking readings with temperature changes.?
I am trying to develop a similar application but I am not getting the desired accuracy. My bigger worry is when I am shorting both the inputs of ADS1230 to ground I am getting high offset of 0x894 and this keeps on changing. Is this a device issue or my board is having a lot of noise?
How do I fix this. Secondly when I connect the load cell I am getting a negative readings of 0xFD1E at no load. I am expecting the load cell to be fully balanced. meaning at no load it should give me a reading same as the offset.
Secondly I am seeing a lot of variation with temperature. The offset varies with temperature
How do i fix this issue.
kind regards
Suchitra
Pin voltages I am using are as follows:-
DVDD = REFP = 3.3V (generated by using TPS71533)
GAIN = 128
SPEED 80SPS