Other Parts Discussed in Thread: ADS7263
Hi,
We have obtained questions from our customers as follows.
Q1. Difference of Half-Clock Mode and Full-Clock Mode
What is the difference of half-clock mode and full-clock mode?
We think that the minimum data throughput in half-clock mode is about 2us,
on the other hand, the minimum data throughput in full-clock mode is 1us.
Is our opinion correct?
Q2. SDOA Only Mode
If we use SDOA only, we think that we should chose half clock mode.
Is it correct?
Q3. Full-Differential Input Mode and Pseudo-Differential Input Mode
Is it possible to set full-differential input mode and pseudo-different input mode in the same chip?
We think that we can not set both modes.
Q4. DVDD Supply Voltage Range
The supply voltage range of DVDD is 2.3V to 3.6V and 4.5V to 5.5V in half-clock mode.
On the other hand, is 2.3V to 3.6V only in full-clock mode.
Is our opinion correct?
Q5. Control of CONVST and RD
If we control CONVST and RD separately, use internal FIFO, we think that it is necessary to set the half-clock mode,
we can not use the full-clock mode.
Is our opinion correct?
Q6. Use two ADS7263
If we convert 4 input analog channel to digial values in the same timing by using two ADS7263,
can we read them from SDOA only?
We think that we can read them by using internal FIFO, controlling CONVST and RD separately and choosing each devices by CS.
Is our opinion correct?
Please tell us about them as soon as possible.
Best Regards,
Kato