I'd like to connect both the ADC and DAC portions of the AFE7225EVM to the TSW1400EVM for evaluation and testing, but I can't find any information on the correct cabling to use. From what I have been told, a physical snap together type connection can be made between one side of the board, but this means I will need a cable to enable the other half of the functionality.
The connectors are made by Samtec but no one over there seems to be able to tell me which cable to use, and my calls to TI support haven't yielded any answers either. Has anyone else been able to connect up these two evaluation boards, and if so, how did you do it?