Hi All,
I'm using an ADS1281EVM on MBBO Motherboard with ADCPro. I am bit confused on how the diffrential input is converted.
I have done the following test : Ain + = 3.28V and Ain - = 1.19V . So i was expecting to read Vout = 3.28V - 1.19V = 2.09V. Instead i read 1.1V, half the input.
So i measured with Ain + and Ain - directly on the ADS1281 pins and it turned out that (Ain+) - (Ain-) = 1.1 V. I have done other tests by changing Ain+ and Ain- , and the input measured directly on ADS1281 pins is always half the input measured on header J6 of ADS1281EVM. Any ideas why?
Thank you
Yannick