Other Parts Discussed in Thread: OPA1664
Hello,
I am using the 14 bit multiplying DAC in an audio application and a fine part it is too by golly.
However I am not realizing the full attenuation at 20 KHz that the graph on page 10 of my data sheet
entitled "reference multiplying bandwidth" promises. For example, if one writes 0010 H into the part, then an attenuation
of -60 dBr should be obtained up to a frequency of 100 KHz or so when capacitance across the part provides
some feedthrough, the graph suggests that about 2 dB will be lost giving an attenuation of -58 dB.
My problem is by the time I get to 20 KHz I am only seeing -54 dB of attenuation. I realize that this is a small
amount of capacitance - my calculation says that is equivalent to about 3.1 pF. I have looked at the pcb layout
and using a rough rule that 1 sq inch at 10thou gap = 100 pF, there is no way that the pcb could account for this
stray capacitance so I have to suspect the part itself. There is a work around that involves neutralizing the 3.1 pf stray with
an external capacitor driven in anti-phase but that is tricky and one would rather the part just performed as advertised.
I am wondering about that pin labeled "VSS" which my data sheet says has no internal connection. If that really
is the substrate of the die, as the name suggests, than leaving it floating as I have done, might cause this crosstalk that
I am seeing. I could try to connect it capacitively to the -15V analog rail ? Any advice would be most appreciated.
Thanks
Dave M