Other Parts Discussed in Thread: ADS5402
I am using the ADS5402 on a custom design card, which interfaces to an FPGA motherboard via high-speed mezzanine connector. I have verified that the ADS5402 works fine when test patterns are selected (via SPI programming). But i always see high spur content on the Ch-A digitized signal (terminating Ch-B into 50Ohm). When i sample Ch-B (terminating Ch-A into 50Ohm), the SFDR is quite close to the datasheet. I provide bandpass filtered, single-tone signals from 10MHz to 500 MHz with sampling rate set to 600MHz for both ADC inputs. When i provide the RF signals to both analog inputs (using a power splitter, and not terminating any analog input), both channels exhibit worse SFDR (approximately 15dB higher than datasheet).
Somehow the Ch-A signal has bad SFDR and that leaks into Ch-B when i provide signals to both inputs. I have tried to isolate the problem by adjusting clock skews (i can provide fine skews to the 600MHz clock) to minimize timing errors. I have also tried a various spi configuration options. It is hard to say if it is a PCB layout issue, as we have done quite a few similar mezzanine cards (different data converters) with high success. Am i missing something with this ADC operation ? I will be happy share my code/ design files if that will help.
Regards,
AB