This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About CW output of AFE5809.

Guru 19645 points
Other Parts Discussed in Thread: AFE5809

Can AFE5809 carry out ON/OFF control of the output for every channel at the time of SCW?
(Although CW output of AFE is added in the latter part, I do not want to add the channel which is not used)

If it can do, please teach me the method.

[Supplement]
Since a noise will increase if the signal of an intact channel is added at the time of SCW reception, the function which turns OFF an intact channel is required.

If it can turn on/off by the register inside AFE, by control of 1ch unit, the noise of an unnecessary channel is removable.

It is expected that there is such a function.

Thank you for your consideration.