Sanjeev,
I agree that an extra amplifier it may be a bit much and maybe unnecessary. We are developing a circuit for the PGA280 and the ADS1259. A cut-out of the PGA/ADS1259 combination is below. This circuit will appear on the EVM, when it is released. We are using the recommended PGA280 filter for the ADS1259 EVM.
There are a few issues to consider when you interface these two devices. The first issue is that the PGA has chopper amplifiers inside and it is important to reduce the output chopper noise at its output. Hence the recommended filter in the data sheet. This filter have been very carefully designed to reduce the chopper noise and maintain PGA208 stability throughout gain changes. The second issue is the corner frequency for the ADS1271. As you might notice, the ADS1271 high frequency speed is approximately 10 times higher that the ADS1259. The corner frequency difference in the PGA filter and the ADS1271 filter is also about 10x, where the ADS1271 filter is 10 times higher. I am not pointing this out to motivate you to use the higher cut-off filter between the ADS1271 and PGA208, rather I want you to know that you need to use the ADS1271 in a high resolution or low power mode. I am hoping that your input signal bandwith will allow this.
Best Regards, Bonnie Baker
----------------------------------------------------------------------------------------------------------- From: Sanjeev Dear Ms. Baker, After following several articles that you have written on sigma-delta ADCs and general advice about dos and don'ts, I wonder if you could comment on a issue that we are having with a new TI part. I have tried to discuss this matter with your technical support department, but to be honest I get the feeling that they are really sure either. We are trying to connect a PGA280 to an ADS1271 for our application. However, the issue regarding the anti-aliasing filter is something that has led to an certain amount of confusion. According to the PGA280 datasheet, a simple two resistor/one capacitor arrangement connected from the PGA's output to the ADC's input should work. However, according to the ADS1271's datasheet and ADS1271EV board, the two resistors are enclosed inside the driving op-amp's closed loop. Using this arrangement, there is a very low output impedance driving the ADC/capacitors. As I believe an extra buffer op-amp is over the top, my question is simply, will the simple two resistor/one capacitor (from the PGA280) approach work well with the ADS1271? With kind regards, Sanjeev
Subject: Sigma delta ADC question