Hi,
I am trying to use the ADS8342 with the schematic setup according to help from a previous post here: http://e2e.ti.com/forums/p/10474/40988.aspx#40988
However, when I power the board up with -5V connected to -DVDD and -AVDD, the ADC pulls about 350mA and runs very... very hot. If I connect these pins to GND however, it only draws about 50mA and is running at a decent temperature. Not completely cold still but it's barely warm. What could cause the chip to do this? I made sure there are no shorts between any of the rails. The other end is 5V for DVDD and AVDD.
I have uploaded a screenshot of the schematic here: http://upload.pixelfaction.com/files/4b1e9402_ads8342.png
(Note: I know C46/48/50/52 are on backwards in the schematic, but I have soldered them the right way on the actual board).
(Note: Also, the input to the DVDD/AVDD area on the top left gets -5V in the schematic, but I corrected this on the board with a jumper. Initially though thtat was the problem, but it still draws a lot of current / gets hot )
Any help would be appreciated.
Thanks,
Aditya