The ads1241 is a 24-bit A/D. I am controlling the A/D with a uP via a SPI interface.
I have having a problem figuring out the meaning of the "Full Scale Resolution" (FSR) registers in the A/D. The register is 24-bits long. My Vcc voltage is 5V and Vref is 1.25V (Vref- is grounded). What is the meaning of the FSR and can someone help with what values need to be written to these registers ? BTW. The highest voltage the A/D would see is approx 55mV, so I'm using a gain of 16 in the PGA. Thanks