This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VSP8133 CCD AFE/TG

Other Parts Discussed in Thread: VSP8133

Note:  I've moved this from the Data Converters >> Video Converters forum to here based on feedback I received.

---

Hello,

 We're designing the Sony ICX692ALA (720p CCD) into several of our camera designs, and I'm looking for an appropriate CCD Analog Front End / Timing Generator to interface with this sensor.

 I've seen the VSP8133 and it looks like it will work, but I'm interested in any reference designs or application notes you may have for this product.

 I only see the datasheet online.

 If you have any reference designs for similar devices that I may refer to (instead of the VSP8133 specifically), that would be helpful too.

 Thank you.

  • Hi, Dear Supports:

    We are going to design a CCD controller (we are new designer in CCD sensor applicatons); the basic specifications are as below listed.

    1. Black/White Interline CCD sensor, i.e. Sony ICX424AL.
    2. Progressive, 640x480 standard pixel; Max pixel clock <37 MHz;
    3. Serial digital output, i.e. LVDS;
    4. ADC accuracy: >=10-Bit;

    My questions are: 

    Q1: VSP8133 is okay? I mean that, VSP8133 is able to cover all controlling to the CCD without any additional IC chips?

    Q2: Is there any similar version of chips other than VSP8133 that is more suitable for our design ( I belive our project is simple)?

    Q3: CouldTI supply us more detailed technical document of VSP8133 or other recommended chips? It will be great if some design examples available.

     Thank you very much.

    Jason Wang