Other Parts Discussed in Thread: ADS1178
Hi,
We are in the process of checking the feasibility to use ADS1178 in Data logger design.
As per the design requirements of the system, sampling frequency is 16 KHz (16 KSPS). Hence the SYNC pin will be connected to a time pulse of 1/16 KHz (= 62.5 us).
We have the following queries in this regard.
- As per the design, we will set ADC in differential input mode, for eight channel simultaneous sampling, and FORMAT[2:0] = 001 (i.e. SPI with TDM in Fixed mode). Is this a feasible mode of operation?
- As the SYNC signal allows for the conversion to be aligned with an external event, we will get samples at every 62.5 us, for all eight channels. Is our understanding correct?
- As per our understanding, the SYNC signal should work as start of conversion (SOC) for the ADC. Hence the ADC shall sample at the frequency on SYNC signal. Is our understanding correct?
- If answer to the above point is yes, then it means we can dynamically vary the ADC sampling frequency by changing the frequency of the SYNC signal. Is our understanding correct? Please confirm.
- We presume that the settling time refers to the time taken by the ADC output to change with respect to a step change at the ADC input. Is our understanding correct?
- In earlier query concerns are raised on the group delay and settling time of ADS1178. How does group delay and settling time impact the sampling frequency? Please clarify.
Your elaborate reply will be of great help to us in feasibility analysis.
Thanks,
Ashwin.