Hi,
I'm using the ADS1243 for TC measurements.
In the data sheet are shown system performanc values with the comment :
(1) Calibration can minimize these errors.
It seems that the given values are the minimized values (with calibration).
What is the initial gain error? I'll use a gain of 64 and have no possibility to adjust the system gain.
regards S.Zimmermann