Other Parts Discussed in Thread: DAC3484
I'm trying to use the DAC3484 EVM rev G with a Terassic DE-4 development board through one of it's HSMC connectors. Beyond the problem of mechanically mating the connectors, based on the schematics available for rev F it appears that the EVM will connect the HSMC power pins in bank 2 and 3 to ground. Would it be possible to connect the EVM to the HSMC connector using a Samtec HQDP cable that would leave the power pins in banks 2 and 3 unconnected? Also are all the signals on Rev G of the EVM routed to the same Samtec connector pins as in Rev F?
Thanks,
John