Other Parts Discussed in Thread: DAC3482, DAC3484
On the Spectrum Analyzer one channel has a -15 dBm per tone fund output and 86 dBc IMD products.
The other channel has a -15 dBm per tone output and 70 dBc IMD products.
Is this an expected behaviour between channels?
Or what could I be doing wrong?
Each arm of the DAC3482 output is terminated with 50 ohm resistors, together with shunt 390nH pull down inductors. There are 100pF DC blocking caps at each output port.
DAC Rate=1228.8Msps
Mixer ON, NCO=OFF.
Two tone output 5 MHz separation 180&185 MHz
4x Interpolation
0 dBFS
QMC=OFF
Thanks in advance.
Sefa