Other Parts Discussed in Thread: ADS1148
There has been a problem with our ADS1148 based temperature measurement circuit (see above) while practically
using it in our product.
We have been using it for RTD measurement (Ratio-metric conversion based on 330 ohms reference resistor) without any problem. For Thermocouple measurement, we simply remove the jumpers joining the AIN1,AIN3,AIN5 and AIN7 so that four thermocouples could be independently measured by differential configuration. (AIN0-AIN1 for TC0, AIN2-AIN3 for TC1, AIN4-AIN5 for TC2, AIN6-AIN7 for TC3).
We have pumped in a few milli volts using external power supply into the differential channels to test our register configurations and linearization calculations. The values are all correct.
However, when we really put in the Grounded thermocouples on the heating system where the thermocouple probe is connected to the Earth wire of the power, the readings stays low around zero even at the higher temperature.
When I removed the Earth wire connection to the thermocouple probe, the readings increase proportionally as the system is heated up.
What really puzzled me here is that the ADS1148 circuit ground has no connection to the Earth wire of the AC mains yet connecting Earth wire to the thermocouple probe would still affect the measurements somehow.
Please suggest me ways to make the ADS1148 circuit configuration right with the grounded thermocouple. I can't use the un-grounded thermcouples in our product. We have to try to find a way to make ADS1148 work with the grounded thermcouple connected to Earth wire. (while the DC supply ground for ADS1148 is isolated from Earth)