Other Parts Discussed in Thread: TLV5608
Datasheet is here http://focus.ti.com/lit/ds/symlink/tlv5608.pdf
I've been confused for a long time.when i select any one channel,all of 8 channels have same analog output,and the voltage value is reasonable.However high 4 bits (0000-0111)indicate the channel 1-8 respectively,and the low 12 bits (d1,d0 are ignored)indicate the digital value needed to be converted,these 16 bits are sent together.
The MCU oscillator is 12 Mhz,and the program:
void DAC_Tlv5608(const unsigned int chan_sel,const unsigned int tem_value)
{
unsigned char i = 0;
unsigned int write_value = 0;
write_value = ((chan_sel<<12) | (tem_value<<2));
LDAC = 0;
FS = 1;
FS = 0;
for( i=0; i<16; i++)
{
if(write_value&0x8000)
{
DIN = 1;
}
else
{
DIN = 0;
}
SCLK = 1;
write_value <<= 1;
SCLK = 0;
}
LDAC = 1;
FS = 1;
}
How does this problem occured commonly?
Thank you very much for your reply.
Tim