This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1203 - 1bit or 16 bit?

Other Parts Discussed in Thread: AMC1203, ADS1202, AMC1210

  • 1-Bit, 10MHz, 2nd-Order, Isolated Delta-Sigma Modulator (Rev. A) (PDF, 708 KB) 3583 views
    10 Mar 2009
  AMC1203
Resolution(Bits) 16  
  • Hi Dmitron,

    The AMC1203 is basically the modulator section of a normal Delta-Sigma converter.  The output from this device is a serial data stream which would need to be put through a digital filter.  You can achieve 16-bit resolution by using a sinc3 filter with a decimation ratio of 256.  The filter portion could be built using an FPGA or with an off the shelf chip like the AMC1210.  There are details on the VHDL available for FPGA implementation off the 'Reference Design' link from the ADS1202 product folder:

    http://focus.ti.com/docs/toolsw/folders/print/ads1202ref.html