Other Parts Discussed in Thread: TLV5631, TLV5637
Hi,
If I use the internal voltage reference is there anything I need to do to the REF pin - leave floating or add a small cap?
Cheers
Calum
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Calum,
Based on what I see in the TLV5631 Data Sheet on page 4, you should have 10 uF in parallel with .1 uF on the ref output pin.
Thanks Jeff,
Looking at page 5 of http://www.ti.com/lit/ds/symlink/tlv5637.pdf it indicates a max load capacitance of 100pF only. But I assumed this value is only if you are using the internal reference to drive another device? I am only using the ref internally (not using it to drive another device)so do I need to do anything with the Ref pin?
Cheers
Calum
Hmmm....Somehow I think that the ref circuits in the 5637 and 5631 are the same but the Load C specs are different. In the 5631 DS it says...
"A decoupling capacitor must be connected to the REF pin if internal reference is selected to ensure output stability.A 1 mF to 10 mF capacitor in parallel to a 100 pF capacitor should be sufficient, see Figure 13."
I'll let BU Apps. for these devices clear this up.
Hello,
These TLV products are quite old and I do not have any documentation available concerning the reference connection for the TLV5637. Based on the functional block diagram for the device I do not see any need for extra decoupling, especially since this is only a 10-bit part, as the bandgap voltage is buffered and driving two more high impedance buffer stages.
What's the application for this part? Are there particular concerns for additional reference decoupling?
Hey Kevin,
When you say extra decoupling what do you mean? Should there be a 10uF in parallel with 100pF, should there be 100pF only or should there be no external decoupling?
Cheers
Calum
Calum,
Sorry for the lack of clarity; I'm saying that based on my own intuition I do not believe there should be any requirement for external decoupling.
If you've observed something to the contrary, though, I can certainly try to build something up to check it out. This part doesn't have an evaluation kit, though, and the characterization setups are long gone - so it may take a while to get something ready.