Other Parts Discussed in Thread: AFE4400, OPA380, AFE4490
Hello,
I am planning to build a reflective pulse oximetry.I used AFE4400EVM board as an experiment for studying oxygen saturation and pulse measurements.
Could some one give the suggestions of which model of LED,specific photodetector and the OP-AMP, the value of resistor (feedback) , capacitor(if any) needed for the transimpedance stage. Planning to read the ADC value out from the OP-AMP through a microcontroller MSP430.
And also if anything else is needed for the reflective pulse oximetry design.
Thanks in Advance.