This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1292R - Question

Other Parts Discussed in Thread: ADS1292

Hello,

Please support of customer question for ADS1292 and refer to the below. 

>Refer to the ADS1292-EVM schematic<Fig-1>. Is this 2-ECG and 1-Respiration function available?

  I understand only 1-ECG&1-RES.or 2-ECG available.

>Where I can find basic information of input signal between Respiration and Hear rate?

>As I know, LA(left ARM) & RA(right ARM) have to located at right position.

  Can I get the same measurement if I locate them by switching (LA to RA location, RA to LA location)?

> Is there any difference on algorithm if ADS1292 measures using Single end or Differential mode?

<Fig-1>

 

 

from Eddy

(eddy.lee@avnet.com)