This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1256 + 6416T still can not work.

Hi TI,

   After reconfigure my board, my program is still be blocked by the TTIDCSTATUS WaitDrdy(TADS1256 *pADS). It is the function call from the dc_configure() in my main.c.

   I am wondering What else I should do in addition to configuring DCP generator and modify the .cdb file by adding _DCPDISP_dispatchEdmaIsr? I mean, do I need to add any function to configure the External Interrupt #5 for ADC board or configure the timer?

   I wanna upload my project file to any TI engineers. Could any one give me your email, tonylou.tw@gmail.com.  Hope TI engineers can take a look on my program and test it. This simple program directly copied from the DCP tutorials is supposed to work.

   Thanks.

Following is the hardware setting and DCP software setting.   
 
--- DCP Software Setting
Default Setting except one: I choose Intertupt as Ext Int 5.
Because the DC_INTb (5-6k) ---(Pin 48)--- DC_EINT5 (6416T)

--- Hardware Setting on the ADC board

Top position on the 5-6K Interface Board, which means connection with J16.

S1 ( AIN0-1 Input Select Switch ) -  Middle position of the switch, which makes AIN0 connected to +2.5V and AIN1 connected to Ground.
S2 ( AIN2-3 Input Select Switch ) -  Middle position of the switch, which makes AIN2 connected to +2.5V and AIN3 connected to Ground.
S3 ( Reference Input Select ) - Up position of the switch, which makes VRP connected to +2.5V and VRN connected to AGND.
S5 ( System Clock Select ) - Left position of the switch, which means digital power supply is onboard 7.68MHz crystal.
J4 - default setting - Short the pin #1 and the pin #2. Short the pin #3 and the pin #4.
J6 - SYNC'/PWDN' - Short SYNC'/PWDN' with DVDD
J7 - RESET - Short RESET' with DVDD
J8 - CS - Short CS with GND
J9 - default setting - Don't short any pins.
J10 - default setting - Short the pin #1 and the pin #2. Short the pin #3 and the pin #4. Short the pin #5 and the pin #6.

Chun-ming (Tony)

  • Tony,

    The settings for the EVM are OK, but the interrupt used is interrupt EINT6. If you look at the schematic, EVM_INTb goes to W9 and has the signal name DC_INTc afterwards, which connects to pin 67 of the J19. Pin 67 is DC_EINT6 on the C6416 DSK.

    I'm going to send you an example project to your e-mail address, which should work for you. Please have a look at the main.c file, as the header describes the correct jumper settings on the 5-6K interface card as well.

     

    Richard