Other Parts Discussed in Thread: ADS6425
I am using the ADS6425 and I have some questions regarding the reference voltage. I am using the internal reference and it is not clear to me how to calculate the LSB size in volts. Normally I would take the reference voltage and divide by the number of bits, in this case 4095 since it’s a 12bit converter. However this part has a "top" reference voltage of 2V and a "bottom" reference voltage of 1V. So do I take 2V/4095 or 1V/4095?
Furthermore, table 19 shows some gain settings vs. input voltage. I assumed there is some amplifier that will increase the signal amplitude sent into the converter, and so consequently the maximum signal amplitude applied to the converter has to be reduced when there is a gain applied inside the ADC.... correct? If I use a gain setting, does this have any impact on the VREF or LSB size? Or is the size of my LSB the same regardless of if I set the ADC with a gain or not.