I'm designing the ADC12D1800RFIUT analog inputs. I've decided that I'm using a balun input device from Anaren, part number B0430J50100AHF. This balun has a balanced output and seems like a good device for my application. The issue is that the ADC analog inputs for the positive and negative input pins are swapped at the ADC device. Reference input pins H1=VinIP, J1-VinIN, N1=VinQP and MVinQN.
N1 - VINQP
M1- VINQN
J1 - VININ
H1 - VINIP
When performing the PWB layout the issue is that since the ADC inputs P and N and essentially swapped for the I and Q inputs and the balun interface crosses for one of the inputs. I belive that pin 6 on the balun is the high side and pin 4 is the low side of the balun outputs. I'm attempting to keep the analog input layout from the balun to the ADC identical but if I need to add vias to one balun output interface to the ADC then the circuitry is different. Can you suggest a layout that works with the Anaren baluns?
Thans,
Randy