This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VHI from ADS1254 is too low

Other Parts Discussed in Thread: ADS1254

Hi every body  I've got a problem, The DRDY V-high from the ADS1254 is to low. I think it should be 3.3 V but its just 100mV so de microcontroler (18F26J50) doesn't sense the falling edge, so It keep waiting till the event occurs.

Please help me Idon't know why.

the coupling resistance is 1 MOhm, if I put a weaker resistance, the signal DRDY has an offset why?

best regards

  • Hi Jose,

    The spec you want to look at is "VOH" the output high voltage. For the ADS1254, it is a minimum of DVdd - 0.4 V, or 2.9V for a 3.3V DVdd.

    Regarding the 100mV output, do you have schematic you can share showing the connection?

    Best Regards,
    Chris