This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1217: current that Dout output (pin 36) can be drained (IOL)

Other Parts Discussed in Thread: ADS1217

We use the ADS1217IPFB ADC in many of our products.

Now we have found a problem with the speed of propagation of the optocouplers we use to isolate the SPI bus to communicate with the microcontroller.

We have read the datasheet of ADS1217IPFB but we don't find a data. We need to know which is the current that Dout output (pin 36) can be drained (IOL) .We only know the VOL value when the current draw is 1 mA (page 5 of the datasheet).

We would need to know which is the typical value and maximum drain current of the output Dout. Now we use 3mA, but we would like to use 10mA. Is it possible?