Other Parts Discussed in Thread: MSP430F5338, ADS805
I'm using the ADS805 with an MSP430F5338 and was wondering what is the correct way to obtain a valid sample. Currently, I am using a pre-scaled version of SMCLK from the MCU as the clock input for the ADC (around 20kHz). However, I haven't been able to read an accurate sample. How do I know when the output of the ADC is valid? When should the MCU read the ports to which the ADC is connected?
Thanks