This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS 1292 data sheet question

Hello,

in page 7 table 1.  when PGA gain = 1.

ENOB = 2 log (VREF/( sqrt(2) * Gain * RMS Noise))  ,     Equation 3.

if I use the data in table 1.

2* log ( 2.42V / 1.414 * 1* 1.5 uV)  = 12.11

so ENOB is 12.11, why the ENOB in table 1 is 20.1. do I misunderstand anyghing here?  appreciate your help.

I always confuse with the relation about ENOB, SNR. which book or artical or paper clearly explain the ADC parameters?

David

REGISTER (SPS)   (Hz)     μVRMS    μVPP     SNR    BITS       ENOB
000              125    32.75     1.5          10.3        121.0    18.83    20.10